The following instructions are a step-by-step
guide for connecting the device to a computer and evaluating the performance of the
device.
- Connect the device EVM to the PHI board. Figure 6-1 indicates where the screws are to be installed.
- Use the provided USB cable to connect the PHI to the computer.
- LED D5 on the PHI lights up, indicating that the PHI is
powered up.
- LEDs D1 and D2 on the PHI start flashing, indicating that
the PHI is booted up and communicating with the PC.
- Launch the device EVM GUI software from the installed path, as
Figure 6-2 shows, or by using the desktop shortcut created during installation.