SBAU407 april   2023 ADS8354

 

  1.   Abstract
  2.   Trademarks
  3. 1Overview
    1. 1.1 ADS8354EVM-PDK Features
    2. 1.2 ADS8354EVM Features
    3. 1.3 Related Documentation From Texas Instruments
  4. 2Analog Interface
    1. 2.1 Connectors for Analog Inputs
    2. 2.2 ADC Input Signal Driver
      1. 2.2.1 Input Signal Path
  5. 3Digital Interfaces
    1. 3.1 SPI for the ADC Digital I/O
  6. 4Power Supplies
    1. 4.1 ADC Input Driver Configuration
    2. 4.2 ADC Voltage Reference Configuration
  7. 5ADS8354EVM-PDK Initial Setup
    1. 5.1 Default Jumper Settings
    2. 5.2 EVM Graphical User Interface Software Installation
  8. 6ADS8354EVM-PDK Operation
    1. 6.1 EVM GUI Global Settings for ADC Control
    2. 6.2 Time Domain Display Tool
    3. 6.3 Spectral Analysis Tool
    4. 6.4 Histogram Analysis Tool
  9. 7Bill of Materials, Printed-Circuit Board Layout, and Schematics
    1. 7.1 Bill of Materials
    2. 7.2 PCB Layout
    3. 7.3 Schematics

Time Domain Display Tool

The Time Domain Display tool provides a visualization of the ADC response to a given input signal. This tool is useful for both studying the behavior and debugging any gross problems with the ADC or front-end drive circuits.

As per the selected interface mode settings using the Capture button indicated in Figure 6-4, the user can trigger a data capture of the selected number of samples from the ADS8354EVM-PDK. The sample indices are on the x-axis, and two y-axes show the corresponding output codes and the equivalent analog voltages based on the specified reference voltage. Switching pages to any of the analysis tools described in the subsequent sections triggers calculations to be performed on the same set of data.

GUID-20230223-SS0I-PQS3-ZCRW-DJDZC7JKDL2F-low.svgFigure 6-4 Time Domain Display Tool Options

Both channel A and channel B waveforms are displayed in Figure 6-4. These channels are identical and overlapped.