SBAU408 august 2023 ADS7953
The ADS7953 is a low-power, 16-channel, SAR ADC that supports single-ended analog inputs. The ADS7953EVM uses an OPA192 to drive optional paths such as channel 15 and the AINP pin of the ADC. The ADS7953EVM is designed for easy interfacing to various analog sources. This section describes the front-end driver circuitry details, including jumper configurations for the analog input signal source.