SBAU409A September   2022  â€“ November 2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Overview
    1. 1.1 ADS9218EVM-PDK Features
    2. 1.2 ADS9218EVM Features
  4. 2Analog Interface
    1. 2.1 ADS9218 Device Connections
    2. 2.2 ADC Differential Input Fully Differential Amplifier (FDA)
    3. 2.3 Common Mode Amplifier Drive
    4. 2.4 Voltage Reference
  5. 3Digital Interface
    1. 3.1 Clock Connection
  6. 4Power Supplies
  7. 5ADS9218EVM Software Installation
  8. 6EVM Operation
    1. 6.1 USB Driver Installation
    2. 6.2 Connecting the Hardware and Starting Software
    3. 6.3 Optional Connections to the EVM
    4. 6.4 Initial Required Setup on the Config Tab
    5. 6.5 Initial Required Setup on the Capture Tab
  9. 7Bill of Materials, Schematics, and Layout
    1. 7.1 Bill of Materials (BOM)
    2. 7.2 Schematics
    3. 7.3 Layout
  10. 8Revision History

USB Driver Installation

This section describes the steps for installing the USB driver.

  1. For the TSWDC155, connect J8 to the workstation using a USB-C to USB-A cable
  2. Open the Windows® Device Manager, as shown in Figure 6-1, and right-click on the WestBridge folder in the Device Manager window and select the Update Driver button (see Figure 6-2)
  3. In the next window that appears, select Browse my computer for driver software
  4. Then select Let me pick from a list of available drivers on my computer in the next pop-up window
  5. Click on Have Disk in the pop-up window and navigate to C:\Program Files\Texas Instruments\ADS92xx\bin\proj_lib\Sparrow\Bootloader (see Figure 6-2).
Figure 6-1 Open Windows Device Manager
Figure 6-2 Update Driver with Device Manager