SBAU409A September 2022 – November 2022
The ADS9218 has a common-mode output pin (VCMOUT). The common-mode signal must be buffered to drive the THS4552 common-mode input pin. Figure 2-3 shows an example of the buffer circuit. R35 bypasses the amplifier and is not populated. When R35 is populated, U8 is unpopulated so that the ADC VCMOUT pin directly drives the FDA VCM input.