SBAU411 February 2023 ADS127L21
#GUID-1D7DB8D7-0785-4286-A5C2-A87F108D63B7 shows the user-programmed filter response. This frequency response includes all upstream filter stages in the ADS127L21. The filter response allows for a quick visual check of the desired filter.
There are several prebuilt filters available that can be downloaded to the ADS127L21. These prebuilt filter files can be used as a template for custom filter designs when using the EVM GUI to download to the ADS127L21. The prebuilt filters are copied to the C:\Users\Public\Documents\Texas Instruments\ADS127L21\Configuration Files\Coefficients\ directory when the EVM GUI is installed.