SBAU416B November 2022 – January 2024 ADS9813
In Figure 6-6, shows an example data capture display. In this step, the necessary updates to the Capture settings are made to capture the time domain data and to get a good frequency domain result. First, the EN SYNC button is clicked to generate a synchronization (SYNC) signal. The SYNC signal is only required once during power-up. The SYNC signal resets the internal analog channel selection logic and aligns the FCLKOUT signal to the data frame. Next, update the number of samples to at least 32k to get good frequency domain results (for example, accurate FFT display, SNR data, and THD data). Finally, select the Hanning type window to eliminate spectral leakage in the FFT result.
When these changes are made, press the Start Capture button to collect time domain and frequency domain data. Select the appropriate tab to view data for channel 1 or channel 2.