SBAU416B November 2022 – January 2024 ADS9813
After the EVM GUI is started, press the following buttons in the order shown in Figure 6-5 below. Confirm that each step is completed before proceeding by monitoring the Status message. For the Power Up and Program FPGA buttons, some status LEDs on the hardware illuminate. After all four buttons are pressed, the power on the ADS9813EVM or ADS9817EVM is on and the ADS9813 or ADS9817 device registers are configured.