SBAU419 November 2022 TMAG5170
The Magnetic Sense Enhanced Proximity Tool is built in Python using a simple graphical user interface, which prompts the user for design information regarding the magnetic material, magnet shape, type of motion, sensor location and sensor type. Successful simulations will produce a 3D animation showing the motion of the magnet relative to a sensor marker. The orientation of the magnet and sensor may be adjusted to model many basic motion types. These include axial, joystick and hinge rotations as well as linear travel. It is also possible to capture the magnetic field vector components at a single sample location.