SBAU419 November 2022 TMAG5170
Spherical magnets are created in the tool by selecting "Sphere" for Magnet Shape. This magnet type is a dipole magnet and only requires that the user enter the diameter in the Magnet Geometry section.
Spherical magnets can be difficult to align properly during installation, but provide the best overall symmetry in magnetic field. As a result they may be used to track tilt and rotation common in joysticks if the challenge of alignment can be resolved.