SBAU419 November 2022 TMAG5170
Axial cylinder magnets are similar in nature to a diametric cylinder in that both magnets only have a single pole pair (2 poles). Magnet shape is defined using the same input parameters, but instead of showing polarization across the diameter of the cylinder, the polarization is along the axial length of the magnet. The default polarization for this magnet is in the Z-direction.
These magnets can be found in various lengths, and this length is a major factor in the overall field strength produced by the magnet. Often, coin shaped magnets are used to observe linear displacement and when the magnet approaches the sensor head-on.