SBAU435 February 2024 ADS127L18
The ADC Capture Settings page allows easy configuration of multiple ADC settings and is an alternative method to using the Register Configurations page. There are multiple tabs on the ADC Capture Settings page, including ADC, Clocking, SPI and Data Port, Filter, and Channel. Changing these settings also updates the values on the Register Configuration page. These tabs are discussed in more detail in the following sections.