SBAU436A January 2024 – February 2024
Connect differential input signals directly to the ADC on channels 5-8 using the input headers. These channels are connected to the device pins though a small charge bucket filter to counteract the effects of the inrush current on the device. Similar to Section 2.1.1, apply single-ended signals to these headers by grounding one of the input pins. Figure 3-2 shows an example of the undriven input pin headers and associated charge bucket circuitry for channel 5.