SBAU436A January 2024 – February 2024
Figure 3-5 shows the fully differential amplifier (THS4551) circuit used to drive the ADC. The input applied to AINP and AINN must be a low-distortion differential signal. Pin 7 on U13 (VOCM) controls the common-mode output for the amplifier, and is set by the ADS1278 VCOM output (pin 55). The feedback network includes a low pass filter (R74, R78, R94, R91, C36, and C52). The amplifier output connects to an RC filter that connects to the ADC input (R37, R43, C30, C26, and C32). The amplified configuration has several do-not-populate (DNP) components that provide flexibility, but are not required for good performance. The amplifier power supplies are connected by default to the AVDD and GND supplies that are also used for the ADC.