SBAU436A January 2024 – February 2024
The onboard PLL of the PHI controller board provides the default clock for the ADS1278 EVM. This clock is configurable for arbitrary frequencies using the Clock Settings dialogue in the GUI as described in Section 4.3. The ADS1278 EVM can also be configured to use an onboard hardware oscillator or an external clock. Figure 3-8 shows the different on-board clock options for the ADS1278 EVM.
When jumper JP2 is in the default position (1-2), the CLK pin on the ADS1278 is routed to the PHI clock output. Change the shunt on jumper JP2 to position 2-3 if the ADS1278 EVM is used with the onboard clocking options. Moving jumper JP1 to position 1-2 disables the local 27MHz oscillator (Y1) on the ADS1278 EVM, allowing an external clock supplied on the SMA connector (J7).
To use an external clock source, apply a CMOS square-wave signal with an amplitude equal to IOVDD (3.3V) and a frequency within the specified range of the ADS1278. Additionally, the appropriate clock frequencies must be programmed into the Clock Settings dialogue in the GUI to verify the communication speed is correct.