SBAU439 January   2024

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Analog Interface
      1. 2.1.1 ADC Channel Inputs
        1. 2.1.1.1 High-bandwidth, Fully-Differential Circuit: THS4551
        2. 2.1.1.2 Precision, High-CMRR Circuit: PGA855
      2. 2.1.2 Voltage Reference
    2. 2.2 Power Supplies
      1. 2.2.1 USB Power and When to Power the Board Externally
    3. 2.3 Digital Interface and Clock Inputs
      1. 2.3.1 Digital Interface Connections
      2. 2.3.2 Clock Select
    4. 2.4 ADS9227EVM Quick Start Guide
  9. 3Software
    1. 3.1 ADS9227EVM Software Reference
      1. 3.1.1 ADS9227EVM-GUI Software Installation
      2. 3.1.2 USB Driver Installation
      3. 3.1.3 Using the CONFIG Tab
      4. 3.1.4 Using the Capture Tab
      5. 3.1.5 Using the INL/DNL Tool
      6. 3.1.6 Using the Histogram Tab
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1.     Trademarks
  12. 6Related Documentation

USB Driver Installation

This section describes the steps for installing the USB driver.

  1. For the TSWDC155EVM, connect J8 to the workstation using a USB-C to USB-A cable.
  2. Bypass any USB hub and connect directly to the computer.
  3. Open the Windows® Device Manager, as shown in Figure 4-3, and right-click on the WestBridge folder in the Device Manager window and select the Update Driver button (see Figure 4-4).
  4. In the next window that appears, select Browse my computer for driver software.
  5. Then select Let me pick from a list of available drivers on my computer in the next pop-up window.
  6. Click on Have Disk in the pop-up window and navigate to:
    1. C:\Program Files\Texas Instruments\ADS92xx\bin\proj_lib\Sparrow\Bootloader
GUID-20221027-SS0I-N950-WDC6-TSZL3RSGGRG3-low.pngFigure 3-3 Open Device Manager
GUID-20221027-SS0I-VBGD-2JMK-HJVR83FZHZDZ-low.pngFigure 3-4 Update Driver With Device Manager