SBAU441 March   2024

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Board Overview
    2. 2.2 Required Equipment
    3. 2.3 Hardware Setup
  9. 3Software
    1. 3.1 Required Software
    2. 3.2 Software Setup
  10. 4Implementation Results
    1. 4.1 Evaluation Setup
    2. 4.2 Data Capture
  11. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layouts
    3. 5.3 Bill of Materials (BOM)
  12. 6Additional Information
    1. 6.1 Trademarks
  13. 7References

Hardware Setup

  1. Connect the ADC3669EVM to the TSW1418EVM via the FMC connectors.
  2. Connect the USB Mini-B connector (J5) on the ADC3669EVM to your PC using the USB Mini-B Cable provided in the EVM kit. The AD3669EVM is powered via USB, so there is no need to provide external power.
  3. Connect the USB Mini-B connector (J2) on the TSW1418EVM to your PC using the USB Mini-B cable provided in the EVM kit.
  4. Make sure the PWR SEL headers (J10 & J13) on the TSW1418EVM have jumpers installed as followed:
    Table 2-1 TSW1418 Jumper Configuration.
    Header Jumper Position
    J10 Pins 2-3
    J13 Pins 1-2

    This configures the TSW1418EVM for power via USB, so there is no need to provide external power.

  5. Connect the Micro USB Cable to the JTAG dongle and connect the JTAG dongle to the JTAG header (J3) on the TSW1418EVM. Then connect the Micro USB Cable to your PC.
  6. Using an SMA cable and an inline 500MHz band pass filter, connect the signal generator to the SMA connector labeled CLK (J3) on the ADC3669EVM. Set the signal generator’s output signal frequency to 500MHz and the signal amplitude to +10dBm.
  7. By default, the EVM is configured to take a single ended input, so analog inputs must be applied to connectors AINp (J2) and BINp (J4) on the ADC3669EVM. Using an SMA cable and an inline 10MHz band pass filter, connect the signal generator to analog input channel A (J2). Set the output signal frequency of the signal generator to 10MHz and the signal amplitude to roughly +10dBm.

Figure 3-2 shows what the user's setup looks like.

GUID-20240118-SS0I-QDCH-X6H4-B392JJCKWTCG-low.svg Figure 2-2 Assembled setup of the ADC3669EVM