SBAU447 May 2024
Figure 3-4 shows the example single-ended output with fixed gain output circuit for the DIYAMC-0-EVM.
Row 2 of the EVM provides a single-ended analog output with fixed gain. Using Coupon A2 as an example, the output is accessible to the user by connector J4. The passive components of the output are comprised of R6 and C16 that form an RC filter from pin 7 of the device with a cutoff frequency of 159MHz. The VOUTN pin is tied to ground in this configuration since the pin does not have an output. C13 and C14 serve as decoupling capacitors for noise reduction and low-side supply (VDD2) stability.
Using an oscilloscope, the user can observe the output signal at J4.2 (VO).