SBAU448 September 2024 ADS8681W
The Time Domain Display tool allows visualization of the ADS8681W's response to a given input signal. This tool is useful for both studying the behavior and debugging any problems with the ADC or drive circuits.
The user can trigger a capture of the data of the selected number of samples from the ADS8681W, as per the current interface mode settings using the capture button as indicated on Figure 4-5. The sample indices are on the X-axis and there are two Y-axes showing the corresponding output codes as well as the equivalent analog voltages based on the specified reference voltage, the selected Device Range and Voltage Range. The measured maximum and minimum code and equivalent voltage are also shown in the bottom right pane.