SBAU452 March 2024
The TMCS devices are isolated, Hall-effect based current-sense amplifiers that provides ease-of-use and high performance. The TMCS-A-ADAPTER-EVM is a blank PCB intended to provide basic, functional evaluation of all TMCS devices in the DVG, DVF, and DZP packages. The TMCS-A-ADAPTER-EVM is not laid out for electromagnetic compatibility (EMC) testing. The EVM consists of a single printed circuit board (PCB) that has not been populated with any electrical components and must be assembled before use. Included in the EVM kit are the board components required for testing with the EVM as well as high-current lug connectors used for supplying measurement signals to the current sensor.