SBAU456 September 2024 ADS9212
The ADS9212EVM uses single-ended sampling clock for ADC conversions. The positive sampling clock input (SMPL_CLKP) is selected using jumper JP8. Install a shunt in the [2-3] position (default) to source the clock signal from the TSWDC155EVM through the FMC connector. This allows the user to select the clock frequency from the options listed in the EVM GUI.
An external clock source can also be used to control ADC conversions. Connect a low-jitter clock source to SMA connector J14 and install a shunt in the [1-2] position on JP8.
The negative source of the sample clock (SMPL_CLKM) can be sourced from either the FMC connector (FMC_SMPL_CLKM) through R18 or GND through R17, respectively. By default, R17 is populated and R18 is uninstalled.