SBAU467A October   2024  – January 2025 ADC32RF55

 

  1.   1
  2.   Description
  3.   Features
  4.   Applications
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1 Required Hardware
    2. 2.2 Required Software
  8. 3Quick Start Guide
    1. 3.1 Introduction
    2. 3.2 Hardware Setup
    3. 3.3 Software Setup
      1. 3.3.1 ADC32RF5xEVM GUI Installation
      2. 3.3.2 High Speed Data Converter Pro GUI Installation
    4. 3.4 Quick Start Procedure for Bypass Mode
      1. 3.4.1 2x Averaging in Bypass Mode
    5. 3.5 Quick Start Procedure for Complex Decimation Mode
      1. 3.5.1 8x Complex Decimation
      2. 3.5.2 128x Complex Decimation
    6. 3.6 Operating Modes
      1. 3.6.1 Input Comparison
      2. 3.6.2 Quad ADC Mode
  9. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  10. 5Additional Information
    1. 5.1 Trademarks
  11. 6Related Documentation
  12. 7Revision History

Quick Start Procedure for Bypass Mode

Bypass mode is the default operating mode for the ADC32RF5x device family. When operating in this mode, the digital decimation filters that the ADC32RF5x offers is bypassed. Additionally, the user has the option to enable averaging of each internal pair of ADCs per individual channel. Operating in bypass mode without averaging provides the lowest power consumption for ADC32RF5x devices.

TSW14J58EVM

  1. Connect the TRF1305-ADC32RFEVM to the TSW14J58EVM using the FMC connectors.
  2. Connect a 6V, 5A minimum power supply to connector J2.
  3. Connect a USB 2.0 Type-A to Mini-B cable to connector J23.
  4. Connect a USB 3.0 Type-A to micro-B cable to connector J1.
  5. Turn on the power supply and toggle the power switch (SW5) to the ON position. The fan starts spinning and the current draw settles at approximately 2.1A.

TRF1305-ADC32RFEVM

  1. Connect a 12V, 2A minimum power supply to the connector J11.
  2. Connect a USB 2.0 Type-A to mini-B cable to connector J12.
  3. Make sure jumper settings are as detailed in Table 3-1.
  4. Connect a filtered 2.56GHz clock signal (+10 dBm) to input J1 (EXTCLK), then enable the signal generator output.
  5. Connect a filtered 300MHz input signal (-20 dBm) to input J8 (INA), then enable the signal generator output.

GUI Setup

  1. Open High Speed Data Converter Pro (HSDC Pro) and select the TSW14J58. If no device is found, verify that power is on and both USB cables are connected.
  2. Select the device firmware labeled ADC32RF5x_8224_12G-16G and update the firmware by pressing Yes on the pop-up window and waiting for the Downloading Firmware message to finish.
  3. Enter 2.56 G into the ADC Output Data Rate field. A message appears stating New lane rate is 12.8G due to ADC Output Data Rate change. When this appears, press OK.
  4. Enter 300M into the ADC Input Target Frequency field and tick the checkbox Auto Calculation of Coherent Frequencies. Notice that the 300M changes to 300.039M.
  5. Open the ADC32RF5x GUI. Verify that the green USB Status indicator is illuminated as shown in Figure 3-3. If the indicator is red (simulation mode), then verify that the USB cable is connected and that the TRF1305-ADC32RFEVM is powered on and press the Reconnect USB button.
ADC32RF55EVM, TRF1305EVM USB Status Indicator Figure 3-3 USB Status Indicator