SBAU468 September 2024
The analog input circuit for the AMC038XEVM is shown in Figure 2-1.
The high voltage input is accessible through the turret connector (VHV1). The passive components R3 and R6 need to be populated and de-populated, respectively. The components do not need to be modified, and must be kept as is for all device variants. Also, present on the input side are decoupling capacitors. C11 and C12 provide decoupling for the high-side supply, and C7 provides stability for the VSNS node.
Using a signal generator or other voltage source, the user can apply an input signal directly to VHV1. The linear input voltage range of the EVM varies by device selected for the configuration of the user. Reference the device data sheet for more information.