SBOA356 August   2020 OPA1656 , OPA210 , OPA2210 , OPA2320 , OPA2320-Q1 , OPA320 , OPA320-Q1

 

  1.   Trademarks
  2. Introduction
  3. Voltage Offset
  4. Bandwidth
  5. Cascaded Amplifier Bandwidth
  6. Cascaded Amplifier Offset
  7. Multi-Stage Amplifiers
  8. Normal Distributions in Offset Voltage
  9. Noise Considerations
  10. Summary
  11. 10Resources
    1. 10.1 TI Recommended Parts
    2. 10.2 TI Precision Labs Training Videos
    3. 10.3 TI Recommended Resources

Summary

When balancing bandwidth, offset, and noise in a high-gain, multi-stage amplifier:

  • Use the lowest input offset op amps that are practical and cost permits.
  • If different op amps are used in a cascade, use the lowest offset/noise op amp in the first stage.
  • If low offset/noise is the highest priority, apply the highest closed-loop gain in the first stage.
  • If bandwidth is the highest priority, a more even distribution of gain across stages is appropriate.
  • Expect a greater variance in Voso across multiple boards due to Gaussian distributions of Vosi for each stage. Higher closed-loop gain in the first stage will result in less variance.
  • Use small resistor values to keep the thermal noise well below the intrinsic noise of the op amp
  • A low source impedance and a low parallel combination of the feedback resistor network (Req) will reduce the effects of current noise.

As discussed, high-gain applications typically require multiple stages to provide the desired bandwidth and performance. Precision op amps, especially in the early stages of a cascaded amplifier will provide the best performance. The dual-channel op amps recommended below can simplify layout and save board space when multiple stages are necessary.