SBOA412 August 2020 TLV314-Q1
Figure 4-2 shows the TLV314-Q1 pin diagram for the SOT-23 package. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TLV314-Q1 data sheet.
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT | 1 | May cause device to overheat | B |
V- | 2 |
Normal operation, unless dual supply voltage was intended. | D |
+IN | 3 | Input at V- (GND) is valid input, however, desired application result is unlikely. Output goes low if -IN is greater than zero volts. | B |
-IN | 4 | Input at V- (GND) is valid input, however, desired application result is unlikely. Output goes high if +IN is greater than zero volts. | C |
V+ | 5 | Diodes from input to V+ may turn on due to input signal and cause electrical overstress (EOS). Main supply shorted. No power to device. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT | 1 | Output cannot be used by application. | C |
V- | 2 |
Lowest voltage pin will drive V- pin internally via internal diode. | B |
+IN | 3 | Floating input, circuit will likely not function as expected. Output may be high or low. | C |
-IN | 4 |
Floating input, circuit will likely not function as expected. Output may be high or low. | C |
V+ | 5 |
Highest voltage pin will drive V+ pin internally via internal diode. |
B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
OUT | 1 |
V- |
Output shorted to supply. May cause device to overheat. | B |
V- | 2 | +IN |
Input at V- (GND) is valid input, however, desired application result is unlikely. Output goes low if -IN is greater than zero volts. | C |
+IN | 3 | -IN | No damage to device, application circuit will not work. Pins not adjacent to each other. | C |
-IN | 4 | V+ |
Input at V+ is valid input, however, desired application result is unlikely. Output goes low if +IN is less than V+. | C |
V+ | 5 | OUT | May cause device to overheat. Pins not adjacent to each other. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
OUT | 1 | May cause device to overheat. |
B |
V- | 2 |
Main supply shorted to V- (GND). No power to device |
C |
+IN | 3 | Input at V+ is valid input, however, desired application result is unlikely. Output goes high if other input is less than supply |
C |
-IN | 4 | Input at V+ is valid input, however, desired application result is unlikely. Output goes low if other input is less than supply | C |
V+ | 5 | Normal operation if V+ is equal to supply. |
D |