• Menu
  • Product
  • Email
  • PDF
  • Order now
  • Synchronized Measurements with Digital Current Sense Monitors

    • SBOA426 March   2021 INA233

       

  • CONTENTS
  • SEARCH
  • Synchronized Measurements with Digital Current Sense Monitors
  1.   Trademarks
  2. 1Introduction
  3. 2Group Command Details
  4. 3Bench Setup and Group Command Verification
  5. 4Measurement Results and Trade-Offs
  6. 5Conclusions
  7. 6Appendix - Group Command Pseudo Code
  8. 7References
  9. IMPORTANT NOTICE
search No matches found.
  • Full reading width
    • Full reading width
    • Comfortable reading width
    • Expanded reading width
  • Card for each section
  • Card with all content

 

APPLICATION NOTE

Synchronized Measurements with Digital Current Sense Monitors

Trademarks

All trademarks are the property of their respective owners.

1 Introduction

At a high level, digital current sense monitors (also called digital power monitors) consist of an analog front end that is designed to take differential measurements across a sense resistor at a high common mode voltage, an internal analog to digital converter, and a digital output to provide the measurement data to the rest of the system. I2C digital current sense monitors, such as the INA233 (Figure 1-1), offer one shot measurement capabilities which allow the I2C controller (main) to tell the current sense monitor (secondary) to initiate a single measurement. Since traditional I2C communication exists between one main and one addressable secondary on the I2C bus, it is not possible for a single main to initiate a synchronized one shot measurement for multiple secondary devices. However there could be exceptions where commands are provided specifically for this function.

GUID-20210119-CA0I-4FTX-VPJQ-NRWMKP3JT4TT-low.gif Figure 1-1 INA233 Block Diagram

The Power Management Bus (PMBus) is a variation of the System Management Bus (SMBus) which was created for controlling power devices with digital interfaces. Both PMBus and SMBus are based on two-wire open-drain electrical signaling like I2C , but have additional application- specific features. In the case of desiring synchronized measurements between or across multiple digital current sense monitors, a group command exists within PMBus that allows the main to address multiple secondaries sequentially, but execute the command at the same point in time.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale