SBOA444 November 2020 TMCS1100
Refer to the layout guidelines in the TMCS1100, ADS131M08, and LM27662 data sheets.
Note that the order of the AINxP and AINxN pins on the ADS131M08 switches when going from one ADC channel to another.
Minimize the length of the traces used to connect the crystal to the ADS131M08. In addition, there must be clean ground underneath the crystal and placing any traces underneath the crystal must be avoided. Also, keep high-frequency signals away from the crystal.
Use wide traces for power-supply connections.