SBOA510 March 2021 OPA455 , OPA462
An Agilent B2962A or B2912A was utilized as the HV power supply for all of the hardware testing. Custom cables with insulated banana jacks were created to carry power from the supply or SMU to the test board. Any exposed HV connections (such as the banana jacks that plugged into the actual board) were contained within a high-voltage interlock box. For safety, the interlock lid was monitored via a switch connected to the supply or SMU, such that when the interlock lid was opened the supply or SMU output was automatically disabled.