As advanced diagnostics are increasingly being included in various applications, it is often desired to detect when a unique or anomalous event occurs in a system. Example events to detect could include the detection of when a normally closed system is opened, detection of an actuator or control element reaching its end of travel, or even detection of a large external magnetic field. In all of these cases, a simple Hall-effect sensor can often solve this problem in a reliable and robust manner. This article discusses using Hall position sensors to implement a limit-detection function for use cases such as magnetic tamper detection, case tamper detection, and end-of-travel detection.
External magnetic fields may affect magnetically-susceptible components in some systems. Example applications may include electricity meters, gas meters, door and window sensors, cordless power tools, and electronic smart locks. To deal with external magnetic fields tampering with the system, a Hall position sensor can be used to provide an alert to the system when the external magnetic field is beyond a predefined limit. This limit should be selected so that the Hall position sensor detects external magnetic fields before they are strong enough to significantly affect the operation of the system.
To detect strong magnetic fields from either the North or South poles of the magnet, an omnipolar Hall position sensor is often used. The omnipolar sensor will sense limits associated with both polarities of the magnet. In addition, three 1-dimensional Hall sensors arranged across three directions or one 3-dimensional Hall sensor can be used to detect strong magnets across all three dimensions. If only permanent magnets need to be detected, Hall switches are commonly used and the magnetic limit is set by the BOP specification of the Hall switch. However, if an AC magnetic field must also be detected, linear Hall sensors can be used instead. If the system is powered from a battery, a duty cycle mode operation is also common, where the Hall position sensor alternates between active measurement mode and low-power sleep mode to reduce the average current consumption.
As an example, in electricity meters, a strong magnet can paralyze any current transformer current sensors or power supply transformers. As a result, strong magnets are commonly placed on electricity meters to steal electricity. The tampering magnet can be cylinder magnets as shown in Figure 2-1, or even bar magnets. To counteract magnetic tampering, meter manufacturers often use Hall position sensors to detect whenever external magnetic fields are beyond a predefined limit. In some cases, the meter deals with detected magnetic tampering by overcharging the customer as a precaution.
Certain applications implement secure enclosures or casings that are meant to be inaccessible by others. Example applications include electricity meters, gas meters, electronic point of sale (EPOS), set-top boxes (STB), ATMs, and enterprise servers. Often, intrusion attempts such as opening the enclosure or casing must be detected for these types of applications.
One method of implementing this case tamper detection feature is by placing a cylinder magnet on the case and placing a Hall switch directly underneath the magnet, as Figure 3-1 shows. When the case is closed, the Hall position sensor senses that the magnetic flux density is beyond the BOP of the Hall switch. As the case is opened, the magnet will move with the case so that it is further away from the Hall sensor.
As the distance from the magnet and sensor increases, the sensed magnetic flux density decreases. Eventually, the magnet-to-sensor distance would reach a distance threshold that causes the sensed magnetic flux density to fall below the magnetic flux density limit, which would trigger the output state of the Hall position sensor to change and alert the system of the case opening. For this type of detection scheme, the magnetic flux density limit value is set by the BRP specification of the Hall switch. The Hall position sensor should be selected so that its BRP would equal the resulting magnetic flux density when the magnet-to-sensor distance is at the desired distance threshold. There is also some consideration that needs to be made to ensure that the magnetic flux density when the case is closed is far enough away from the magnetic flux density limit to prevent false trips.
Figure 3-2 shows the relationship between BOP, BRP, and the limit threshold for detecting the opening of the case. In this figure, the sensed magnetic flux density is constant until the case is opened.
Hall position sensors can also be used to detect an end-of-travel event for a moving component within a system. Diagnosing when a moving component has moved beyond its intended range of movement is a typical use-case for end-of-travel detection. Example applications for this include the sliding door modules, window modules, roof motor modules, and wiper modules in cars. In this scenario, an axially magnetized cylinder magnet can be placed on the moving component so that it moves with it. For this application, the direction of motion would be opposite to the direction of motion in Figure 3-1 since the magnet will be approaching the sensor instead of moving away from it. A Hall switch can then be used to detect whenever the component and magnet are close enough to the Hall switch. As the magnet gets closer to the switch, the sensed magnetic flux density increases until it increases beyond the magnetic limit. This magnetic limit is set by BOP of the Hall switch. Once the sensed magnetic flux density exceeds the BOP, the state of the Hall switch changes and the system is alerted of this end-of-travel event. The Hall position sensor should be selected so that its BOP would equal the resulting magnetic flux density when the magnet-to-sensor distance is at the desired distance threshold. Figure 4-1 shows the relationship between BOP and the limit threshold for the scenario where the end-of-travel state has been detected.