SBOA551 June   2022 INA240

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2One, Versus Two Reference Pins
  5. 3Bidirectional Current Sense Amplifier Topologies
    1. 3.1 Single-Stage Difference Amplifier
    2. 3.2 Difference Amplifier Input Followed by Noninverting Output Buffer
    3. 3.3 Voltage Feedback Multi-Stage Difference Amplifier
    4. 3.4 Single-Stage Current Feedback
    5. 3.5 Current Feedback Multi-Stage Difference Amplifier
    6. 3.6 Isolated Bidirectional Current Sensors
  6. 4Options for Driving Reference Pins and Input Referred Reference Error
  7. 5Resistor Divider as Reference
    1. 5.1 Resistor Divider and Equivalent Circuit
    2. 5.2 Reference Source Impedance Error in Difference Amplifier
    3. 5.3 Reference Source Impedance Error in Voltage Feedback Multi-Stage CSA
    4. 5.4 Reference Source Impedance Error in Current Feedback Multi-Stage CSA
    5. 5.5 Reference Source Impedance Error in Difference Amplifier with Output Buffer
  8. 6Examples
    1. 6.1 Calculating Reference Source Impedance Error in Difference Amplifier
    2. 6.2 Calculating Reference Source Impedance Error in Voltage Feedback Multi-Stage CSA
    3. 6.3 Calculating Reference Source Impedance Error in Current Feedback Multi-Stage CSA
  9. 7Summary

Isolated Bidirectional Current Sensors

An example of in-package Hall sensors is the TMCS1100 family, shown in Figure 3-6. Within the device, the high-voltage side load current passes through the low-ohmic leadframe path. No external components, isolated supplies, or control signals are required on the high-voltage side. At the low-voltage side, the magnetic field generated by the input current is sensed by a Hall sensor and amplified by a precision signal chain.

Figure 3-6 Bidirectional TMCS1100

The transfer function can be written as:

Equation 6. V o u t _ i d e a l = S × I i n + V r e f _ x

where

  • S is the sensitivity
  • Iin is the target current being measured
  • Vref_x is the reference voltage at the VREF pin

The reference voltage determines the zero-current output voltage. This zero-current output level along with sensitivity determine the measurable input current range of the device, and allows for unidirectional or bidirectional sensing. By shifting the zero current output voltage of the device, the dynamic range of measurable input current can be modified.

The input voltage on Vref pin can be provided by any external voltage source, such as a precision reference IC. The VREF pin is sampled by the internal circuitry at approximately 1 MHz, then buffered and provided to the signal chain of the device. An apparent DC load of approximately 1 µA is observed by the external reference. To prevent errors due to sampling settling, keep the source impedance below 5 kΩ, the level specified in the electrical characteristics table.