SBOA551 June 2022 INA240
Current feedback topology decouples the common-mode input voltage from input bias current and has the potential for high CMRR without precision manufacturing. The current feedback also provides higher bandwidth than its voltage counterpart. As shown in Figure 3-5, the input stage isolates the rest of the circuits from the high input common-mode voltage with high-breakdown MOSFETs. The output stage amplifier common-mode voltage is defined by the first stage load resistors, which converts current into voltage.
The transfer function of the amplifier can be written as: