SBOA551 June 2022 INA240
Rx (kΩ) | C = Rx / (Ri_2 + Rf_2) | m = C / (1 + C) | Err_Vref (mV) | Err_Vcm (mV) | Err_Vdiff (mV) | Err_Total (mV) |
---|---|---|---|---|---|---|
1 | 0.0057 | 0.0057 | –5.68 | 14.20 | 2.84 | 11.36 |
5 | 0.0286 | 0.0278 | –27.78 | 69.44 | 27.03 | 55.56 |
10 | 0.0571 | 0.0541 | –54.05 | 135.14 | 13.89 | 108.11 |
20 | 0.1143 | 0.1026 | –102.56 | 256.41 | 51.28 | 205.13 |
30 | 0.1714 | 0.1463 | –146.34 | 365.85 | 73.17 | 292.68 |
40 | 0.2286 | 0.1860 | –186.05 | 465.12 | 93.02 | 372.09 |
50 | 0.2857 | 0.2222 | –222.22 | 555.56 | 111.11 | 444.44 |
Referring to Figure 5-4 output stage, and using INA240A2 as an example, the design values for input (Ri_2) and feedback (Rf_2) resistors are 50 kΩ and 125 kΩ respectively. Use these nominal values in the calculations shown in Table 6-2. It is known that the common-mode voltage is set at half supply.
Table 6-2 is under the condition of: Vs = 5 V; Vref_x = 1 V; Vdiff = 50 mV.
The common-mode voltage of the output stage is set at half-supply and is independent of the potentially high input common-mode voltage seen at the input of the device. Therefore, the output error term is decoupled from the common-mode voltage of the device. As a result, if the reference voltage is also set at half supply, the two error terms cancel, regardless of the source impedance. However, the term due to differential input still remains. In this table, a 50-mV input to the device input is used as an example, because the front stage is in a gain of 20, the output stage sees and effective differential input of 20 × 50 mV = 1 V.
The second example is INAx191 and INA186. The INA186A2 is used to illustrate. Although the input stage is different from that of INA240, the output stage is very similar. The design values for input (Ri_2) and feedback (Rf_2) resistors are 400 kΩ and 1 MΩ respectively. The common-mode voltage is set at one-third of supply. Again, the nominal values are used in the following calculation.
This information can be used to generate Table 6-3 for the output error terms, under the condition of: Vs = 5 V; Vref_x = 2.5 V; Vdiff = 50 mV.
Rx (kΩ) | C = Rx / (Ri_2 + Rf_2) | m = C / (1 + C) | Err_Vref (mV) | Err_Vcm (mV) | Err_Vdiff (mV) | Err_Total (mV) |
---|---|---|---|---|---|---|
1 | 0.0007 | 0.0007 | –1.78 | 1.19 | 0.36 | –0.24 |
5 | 0.0036 | 0.0036 | –8.90 | 5.93 | 1.78 | –1.19 |
10 | 0.0143 | 0.0071 | –17.73 | 11.82 | 3.55 | –2.36 |
20 | 0.0071 | 0.0141 | –35.21 | 23.47 | 7.04 | –4.69 |
30 | 0.0214 | 0.0210 | –52.45 | 34.97 | 10.49 | –6.99 |
40 | 0.0286 | 0.0278 | –69.44 | 46.30 | 13.89 | –9.26 |
50 | 0.0357 | 0.0345 | –86.21 | 57.47 | 17.24 | –11.49 |