SBOA551 June 2022 INA240
Based on conventional difference amplifiers, this topology achieves input and output functionalities in a single stage. Compared with a conventional difference amplifiers, the most significant distinction is the capability to withstand common-mode input voltage that is significantly higher than device supply voltage while maintaining high gain. For example, the working input common-mode voltage could be 28 V while the device supply is only 3.3 V. Shown in Figure 3-1 is the simplified diagram of such a device. In this diagram, Ri and Rf represent the ideal values of the input and feedback resistors respectively.
The resistor network must be closely matched to achieve good Common Mode Rejection Ratio (CMRR) and Gain Error (GE) performance. The resistor network is often trimmed for matching. Although sometimes it is possible to meet relaxed design goals by optimizing circuit design and layout without trim.
When driving the reference pin of a single-stage difference amplifier, ideally the voltage source should have zero impedance to maintain the balance of the resistor network.The difference amplifier transfer function is the familiar equation: