SBOA551 June 2022 INA240
Figure 5-1(a) shows a resistor divider is used to generate the reference voltage, which is defined by Equation 7 when the contribution from VS is considered:
Figure 5-1(b) shows the Thevenin’s equivalent with the following parameters:
The Thevenin’s equivalent circuit also represents situations where the reference voltage source has finite output impedance. This circuit is used in the next sections.