SBOA571 august 2023 OPA2387 , OPA387 , OPA4387
When measuring current, often shunt-based designs are used. In grid systems, the AC content is 50/60 Hz based and contains the fundamental plus harmonic distortion. For example, in power quality analysis or DC/AC power conversion, the harmonics are analyzed individually to monitor and minimize distortion. The AC carries the main power but an unwanted DC content can be present in addition which must be eliminated by the control loop or detected as an error. Therefore, measuring the DC value at the same time is important. For example, a DC/AC system can generate a 20-A AC current sine wave. At the same time, a 20-mA DC current must be measured. This requirement increases the dynamic range of the system and challenges the analog to digital conversion. Furthermore, the voltage across the shunt can be small such that an external gain stage can be beneficial.