Exceeding the input or output swing limitations on amplifiers causes distortion on the output signal. This document initially covers the basic methods for calculating these limitations. Next, a simplified explanation of how the limitation occurs on internal transistor topology is covered. The internal operation is described to provide insight to the board-and-system level designer on how different categories of amplifiers behave. For example, the operation of two different types of rail-to-rail common-mode range are compared and contrasted. Each of these topologies has specific advantages and disadvantages related to noise and distortion. Finally, the impact of output current on swing limitations, short-circuit protection, and other topics related to the op amp input and output stage are covered.
The practical output voltage range of an op-amp circuit is limited by the power supply voltage, internal op-amp design, and circuit configuration. The output range is always less than the power supply range. Thus, for a ±15-V supply, the output range can be at most ±15 V. From a practical perspective some amplifiers can get very close to the supply limits, but no amplifier actually achieves output swing all the way to the supply voltage. A CMOS rail-to-rail amplifier, for example, can have an output swing a few millivolts from the power supply rail.
There are two amplifier specifications that determine the output voltage range: common-mode range, and output swing from the supply rail. The common-mode range is the range of linear operation of the amplifier versus the input common-mode signal. The input common-mode signal is defined as the average voltage applied to the input of the op amp. However, since the op amp has a virtual short between the two inputs, the voltage is approximately the same on either input. Thus, under normal linear operating conditions, any voltage measured on either input is the common-mode voltage. The common-mode range provides the range of linear operation of the amplifier input stage relative to the power supplies. The output swing range is the range of linear operation for an amplifier output stage relative to the power supply voltage and the load current.
The common mode and output swing specification in
Table 1-1 can be used to determine the input and output range of the amplifier. Use the minimum
and maximum limits from the specification table with the power supply voltages to
determine the input and output range for the amplifier. The OPAx206
Input-Overvoltage-Protected, 4-μV, 0.08-μV/°C, Low-Power Super Beta, e-trim™ Op
Amps data sheet provides two different specification tables: one at
±5 V and one at ±15 V. Since the actual circuit is between these limits, the worst case
is selected. Figure 1-1 provides an example illustrating how the data sheet specification can be applied to a
specific power supply configuration to determine the input and output limitations. In
this example the minimum common-mode limit can be determined by using the negative
supply and minimum limit from the specification table (that is,
(V–) + 1 = (–5 V) + 1 V = –4
V). The maximum can similarly be determined using the 12-V supply
and the table maximum limit (that is, (V+) – 1.4 V = 12 V – 1.4 V =
10.6 V). The same approach can be used to calculate the output
swing limitation. However, in this case the load must be accounted for. In this example,
the load is 10 kΩ, so the output swing is limited by 0.2 V from either supply rail (
–4.8 V < VOUT < 11.8 V). It is also important to realize that this
output limitation is the point that the amplifier is completely nonlinear and the output
is saturated. As you approach the saturation limit, the amplifier output becomes
distorted. Section 9 covers
details explaining the difference between the saturation and linear limit for the
amplifier. The common mode and output swing examples use an asymmetrical power supply
arrangement of VCC = +12 V and VEE = –5 V. In practical circuits
the supplies are more commonly balanced but can be asymmetrical as shown in the example.
The example uses different values for VCC and VEE for instructive
purposes to help identify and differentiate between the two supplies.
Parameter: OPA206 | Conditions | Min | Typ | Max | Unit | |
---|---|---|---|---|---|---|
VCM | Common-Mode Voltage Range | (V–) + 1 | (V+) – 1.4 | V | ||
VOUT | Voltage Output | RL = 10 kΩ, VS = ±15 V | (V–) + 0.2 | (V+) – 0.2 | V | |
RL = 2 kΩ, VS = ± 15 V | (V–) + 0.35 | (V+) – 0.35 | V |
The Introduction showed how the common-mode limitation of the amplifier can be calculated given the supply voltages and the data sheet specification table. The amplifier circuit configuration often determines if this limitation causes nonlinear operation. The voltage follower is the configuration that is most likely to be impacted by common-mode limitations. This is because the common-mode voltage is the same as the input signal and the input signal often covers the entire supply range. Figure 2-1 provides a DC input sweep to illustrate the common-mode limitation of the OPA206 in a buffer configuration. Note that the input voltage is equal to the common-mode signal in this configuration, so the linear range is –4 V to 10.6 V as calculated in Figure 1-1.
The same op amp in a gain configuration is not impacted by the common-mode limitations because the valid input signal range for the gain configuration is small and does not approach the common-mode limits. For example, in a gain of 10 V/V, the input range is ten times smaller than the output range. Figure 2-2 shows the same supply arrangement in a gain of 10 V/V. In this case, the best output range is –5 V to +12 V, so the valid input range is –0.5 V to 1.2 V. Since the common-mode range for this device is –4.0 V to +10.6 V, the valid input signal is never near the common-mode limits. For this example, notice that the output signal does not swing all the way to the supply limits. This limitation is because of the output swing limitations, and not the common-mode limits and are covered in detail later in this white paper.
In the non-inverting configuration, the common-mode voltage is equal to the input signal. For the inverting configuration the common-mode voltage is equal to the voltage applied to the non-inverting input. In general, for inverting amplifiers the non-inverting input is connected to ground or a fixed DC voltage. For inverting amplifiers, the common-mode voltage remains constant regardless of the input signal, so these types of amplifiers generally do not have common-mode issues. The example shown in Figure 2-3 shows that the common-mode signal is held constant at ground, and the amplifier does not experience common-mode limitations. This amplifier has a gain of –1 V/V, so you can substitute this configuration for a buffer configuration if common-mode limitation is a problem for the buffer. However, remember that the inverting amplifier configuration has gain error and drift due to the tolerance of the feedback resistors, whereas the buffer has a very accurate gain of 1 V/V. Furthermore, the resistors add noise and additional power consumption for the amplifier.