SBOA590 November   2024 OPA186 , OPA206 , OPA328 , OPA391 , OPA928

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Input Offset Voltage (VOS) Definition
    1. 1.1 Input Offset Voltage Drift (dVOS/dT) Definition
    2. 1.2 VOS and VOS Temperature Drift Inside the Amplifier
    3. 1.3 Laser Trim to Adjust Performance
    4. 1.4 Package Trim (e-Trim™) to Adjust Performance
  5. 2Input bias current (IB) definition
    1. 2.1 Input Bias Current (IB) and IB Temperature Drift Inside the Amplifier
    2. 2.2 Derivation of IB Conversion to VOS
    3. 2.3 Internal Bias Current Cancelation
    4. 2.4 Super Beta Input Transistors
  6. 3Other Factors Influencing Offset
    1. 3.1 Finite Open Loop Gain (AOL)
    2. 3.2 Common Mode Rejection Ratio (CMRR)
    3. 3.3 Power Supply Rejection Ratio (PSRR)
    4. 3.4 AOL, CMRR, and PSRR Over Frequency
    5. 3.5 Electromagnetic Interference Ratio (EMIRR)
    6. 3.6 Mechanical Stress Induced Offset Shift
    7. 3.7 Parasitic Thermocouples
    8. 3.8 Flux Residue and Cleanliness
  7. 4Zero-drift Amplifiers to Minimize VOS and VOS Drift
  8. 5Calibration of VOS, IB, and Gain Error
  9. 6References
  10. 7Revision History

Common Mode Rejection Ratio (CMRR)

The common-mode rejection ratio (CMRR) for an op amp is defined as the change in VOS versus change in the common mode voltage of the op amp. For an ideal op amp, the common mode signal does not affect VOS (that is, CMRR is infinite). For a practical op amp, however, the CMRR ranges from 60 dB to 170 dB. The equation for CMRR is CMRR = ΔVCM/ ΔVOS or 20log(ΔVCM/ ΔVOS) in decibels.

Figure 3-3 shows a difference amplifier in a gain of 1V/V where the inputs are connected together to force the differential input voltage to zero. The voltage source (VIN) swings from -24 V to +24 V, which causes the common mode voltage (VCM) to swing from -12 V to +12 V. Because the differential input is 0 V (mid-supply), the output remain near zero volts. Finite AOL does not affect the offset (see Section 3.1). Thus, the primary factor impacting the shift in offset voltage is change in the common mode voltage.

The specifications for the OPA210 example are shown in Table 3-1. Based on the specification, you would expect the typical offset to be ±5 µV. Notice the test condition listed at the top of the table indicates that the parameters all assume VCM = VOUT = mid-supply. However, the common mode voltage ranges from -12 V to +12 V, and the output voltage is at 0V. The calculation for a 24V change in VCM voltage shows a corresponding 2.4 µV change in offset (see calculation Equation 31). In this example, the simulated offset shift of 3.85 µV (CMRR = 136 dB) compares well to the calculated shift of 2.4 µV (CMRR = 140 dB). In the simulation notice that VOS = 5 µV specification when VCM = 0 V as you would expect based on the test condition.

Equation 31. ΔVOS=ΔVCMCMRR(lin)=24V10140/20=2.4 μV
OPA206 VOS Shift Due to
                    CMRR on OPA210 Difference Amp Configuration Figure 3-3 VOS Shift Due to CMRR on OPA210 Difference Amp Configuration
OPA206 Simulated Vos and Output Swing
                    for Difference Amp Configuration Figure 3-4 Simulated Vos and Output Swing for Difference Amp Configuration

In many cases, the effects of open loop gain and common mode rejection will be combined as in the case of unity-gain buffer (a follower with G = 1). From a calculation perspective the two calculations can be done separately and the results are combined. Simulation modela both effects and the output reflect the typical operation of the device. In this example, the model shows the slope of VOS due to AOL to be negative and the slope of VOS vs Vcm to be positive. In general, the slope of VOS vs VCM can be either positive or negative, but VOS due to AOL will always have a negative slope. Thus, in this example the two effects are subtracted from each other.

Equation 32. ΔVOS(total calculated)=ΔVCMCMRR(lin) - ΔVOUTAOL(lin)=24V10140/20 - 24V10132/20=-3.63μV
Equation 33. ΔVOS(total simulated)=ΔVOS(CMRR) - ΔVOS(AOL)=3.85μV - 7.59μV=-3.74μV
OPA206 Combined Effects of
                        AOL and VCM on VOS Figure 3-5 Combined Effects of AOL and VCM on VOS