SBOA597 November 2024 OPA928
IB typically can have a logarithmic relationship relative to temperature. This means that as the temperature increases, the IB can be significantly higher. For this reason, highly accurate systems can need to calibrate IB across temperatures. Following is a summary of the steps necessary to achieve ultra-low current calibration. Each step is then described in detail.
In the example, the output voltage (buffer with a gain of ten) moved from +1.0V to -3.4V.
The curve crosses zero volts, and a derivative at the point shows -33.7µV/sec. Assuming the number is the smallest leakage current condition across the capacitor, IB is calculated as -33.7µV/sec / 10.1 gain x 108.6pF x (1-200 x 10-6 x (85-20)) = -357.6aA. The calculation includes the temperature coefficient of the capacitor of -200ppm/°C.
Next, make sure the zero-cross point is away from dielectric relaxation. Calculate the derivative of output voltage over time. The plot of current over output voltage settles at around output voltage closes zero volts. This indicates dielectric relaxation settles at around the output of zero volts. A fitting curve shows -50.5aA/V. The resistance of the integration capacitor is calculated as 1 / (-50.5aA/V) / 10.1 (gain) = 1.96PΩ. The intercept of the fitting curve indicates IB is -354.8aA.
Comparing the number between the intercept of the fitting curve (-354.8aA) and the zero-cross method (-357.6aA) gives a delta of 2.8aA. With that, IB is most likely between -354.8aA to -357.6aA at 85°C.