SBOA597 November 2024 OPA928
One of the methods of measuring a current is using a coulombmeter. A coulombmeter consists of a capacitor within a negative feedback loop. The current is determined by the change in charge on the capacitor over time.
In Coulomb’s law, charge Q is determined by the known value of capacitance C and measured voltage V across the capacitor. See Equation 1.
where:
However, the flow of individual charges is not uniform due to noise and other random variables. One of the advantages of a coulombmeter is that the random flow for a certain time interval is averaged. The resolution of the measurement can be improved as longer integration times are allowed.
Current flow into the inverting terminal of the coulombmeter can create a voltage that is an integration function of the current versus time. Applying current flow into the inverting terminal of the amplifier and the circuit integrates the current over time. The op amp outputs voltage across the integration capacitor. Measuring the change in voltage over a specific time multiplied by capacitance gives current, measured in amperes.
Where: