SBOA597 November 2024 OPA928
Due to the high impedance of a modern amplifier, the circuit has an ultra-high impedance node, and the circuit is sensitive to the movement of the person or an object near the instrument that creates unwanted electrical coupling.
In addition, AC fields, such as the mains line, also influences high-impedance node. When the high-impedance node couples with mains lines with a parasitic capacitance of 1fF, the resulting error current can be 42pA.
An aluminum box shields the high-impedance node from electronic field coupling. Depending on the type of radiation, different material is selected. For inductive coupling, higher permeability material is required.