SBOK051 November 2023 OPA4H014-SEP
PRODUCTION DATA
The OPA4H014-SEP samples, in a biased configuration, were irradiated at a high dose rate of 50-300 rad(Si)/s up to a maximum of 30 krad(Si) and then put through full electrical parametric testing on the production Automated Test Equipment (ATE). Three additional samples were irradiated to 50 krad(Si) for one-time characterization, following the same procedure.
Since the OPA4H014-SEP BICOM-3XHV process technology contains bipolar components, biased and unbiased LDR are also performed, up to 30 krad(Si). Parametric values from HDR and LDR results are compared to determine that the OPA4H014-SEP is not considered Enhanced Low Dose Rate Sensitive (ELDRS).