SBOK052 May 2024 OPA4H014-SEP
The OPA4H014-SEP was biased in a buffer condition, where V+ was set to 9V and V- was set to -9V. On all four channels, the inverting input was connected to the output and the non-inverting input was grounded to midsupply. Current was monitored over time for both V+ and V-. Heavy ions with LETEFF = 43MeV-cm2 / mg were used to irradiate the devices. A nominal flux of 105 ions / s-cm2 and fluence of 107 ions / cm2 were used during the exposure at 125°C. Two runs were completed to provide an overall fluence of 2 × 107 ions / cm2.