The purpose of this study is to characterize the effects of heavy-ion irradiation on the single-event latch-up (SEL) performance of the SN54SC4T08-SEP, a four-channel, two-input positive AND gate with logic-level shifter. Heavy-ions with an LETEFF of 43 MeV-cm2 / mg were used to irradiate three production devices with a fluence of 1 × 107 ions / cm2. The results demonstrate that the SN54SC4T08-SEP is SEL-free up to LETEFF = 43 MeV-cm2 / mg at 125°C.
All trademarks are the property of their respective owners.