SBOK079 October 2023 TPS7H2140-SEP
PRODUCTION DATA
The TPS7H2140-SEP is packaged in a 28-pin HTSSOP plastic package as shown in Figure 3-1. An evaluation board designed for radiation testing was used to evaluate the performance and characteristics of the TPS7H2140-SEP under heavy-ions. Figure 3-2 shows the top view of the evaluation board used for the radiation testing. Figure 3-3 shows the EVM board schematics used for the heavy-ion testing campaign.
The package was delidded to reveal the die face for all heavy-ion testing.