SBOK091 December 2024 OPA4H199-SP
The utilized test facility is the Fast Neutron Irradiation (FNI) Facility of University of Massachusetts Lowell Research Reactor. The neutron fluence for this irradiation was measured utilizing ASTM E-265 “Measuring Reaction Rates and Fast Neutron Fluence by Radioactivation of Sulfur-32” and correlated to the measured reactor power level. All irradiation conditions required under ASTM 722 were met, this includes: neutron fluence, distribution and uncertainty. The Average Integrated Neutron Fluence, 1-MeV(Si) equivalent, reflects these factors. Detailed information of the radiation facility is available at the following link: