SBOS780C March 2016 – June 2021 THS3215
PRODUCTION DATA
The THS3215 is well suited for high-speed, low-distortion arbitrary waveform generator (AWG) applications commonly used in laboratory equipment. In this typical application, a high-speed, complementary-current-output DAC is used to drive the D2S. The OPS of the THS3215 easily drives a 50 MHz, 2.5 VPP signal into a matched 50 Ω load. When a larger output signal is required, consider using the THS3095 as the final driver stage.
A passive RLC filter is commonly used on DAC outputs to reduce the high-frequency content in the DAC steps. The filtering between the DAC output and the input to the D2S reduces higher-order DAC harmonics from feeding into the internal OPS path when the external input path is selected. Feedthrough between the internal and external OPS paths increases with increasing frequency; however, the input filter rolls off the DAC harmonics before the harmonics couple to VOUT (pin 10) through the deselected OPS signal path. Figure 9-2 shows an example of a doubly-terminated differential filter from the DAC to the THS3215 D2S inputs at +IN (pin 2) and –IN (pin 3). The DAC is modeled as two, fixed, 10 mA currents and a differential, ac-current source. The 10 mA dc midscale currents set up the average common-mode voltage at the DAC outputs and D2S inputs at 10 mA × 25 Ω = 0.25 VCM. The total voltage swing on each DAC output is 0 V to 0.5 V.
Some of the guidelines to consider in this filter design are:
Figure 9-3 shows the TINA-simulated filter response for the input-stage filter. The low-frequency 34 dBΩ gain is due to the 50 Ω differential resistance at the DAC output terminals. At 200 MHz, this filter is down 17 dB from the 50 Ω level; it is also very flat through 50 MHz.
In the example design of Figure 9-1, a 50 MHz, third-order Bessel filter is placed between the D2S output and the external OPS input. Another 25 MHz, third-order Bessel filter is placed at the input of a very-high output-swing THS3095 stage. A double-pole, double-throw (DPDT) relay selects the THS3095 path when the internal OPS path is selected in the THS3215. Figure 9-1 shows this design. The key operational considerations in this design include: