SBOS921F December 2018 – November 2023 TMP61
PRODUCTION DATA
Use the TMP61 device along with a voltage reference, and a comparator to program the thermal protection. As shown in Figure 8-10, the output of the comparator remains low until the voltage of the thermistor divider, with RBIAS and RTMP61, rises above the threshold voltage set by R1 and R2. When the output goes high, the comparator signals an overtemperature warning signal. The engineer can also program the hysteresis to prevent the output from continuously toggling around the temperature threshold when the output returns low. Either a comparator with built-in hysteresis or feedback resistors may be used.