Achieving optimum performance with a
high-frequency amplifier such as the THS6222 requires
careful attention to board layout parasitic and external component types. The THS6222RHFEVM can be used as a reference when designing the circuit
board. Recommendations that optimize performance include:
- Minimize parasitic capacitance to any ac ground for all signal I/O pins. Parasitic capacitance, particularly on the output and inverting input pins, can cause instability; on the noninverting input, this capacitance can react with the source impedance to cause unintentional band limiting. To reduce unwanted capacitance, a window around the signal I/O pins must be opened in all ground and power planes around these pins. Otherwise, ground and power planes must be unbroken elsewhere on the board.
- Minimize the distance (less than 0.25 in, or 6.35 mm) from the power-supply pins to high-frequency 0.1 µF decoupling capacitors. At the device pins, the ground and power plane layout must not be in close proximity to the signal I/O pins. Avoid narrow power and ground traces to minimize inductance between the pins and the decoupling capacitors. The power-supply connections must always be decoupled with these capacitors. An optional supply decoupling capacitor across the two power supplies (for bipolar operation) improves second-harmonic distortion performance. Larger (2.2 µF to 6.8 µF) decoupling capacitors, effective at lower frequencies, must also be used on the main supply pins. These capacitors can be placed somewhat farther from the device and can be shared among several devices in the same area of the PCB.
- Careful selection and placement of external
components preserves the high-frequency performance of the THS6222. Resistors must be of a very low reactance
type. Surface-mount resistors work best and allow a tighter overall layout.
Metal film and carbon composition, axially-leaded resistors can also provide
good high-frequency performance.
Again, keep leads and PCB
trace length as short as possible. Never use wire-wound type resistors in a
high-frequency application. Although the output pin and inverting input pin
are the most sensitive to parasitic capacitance, always position the
feedback and series output resistor, if any, as close as possible to the
output pin. Other network components, such as noninverting input termination
resistors, must also be placed close to the package. Where double-side
component mounting is required, place the feedback resistor directly under
the package on the other side of the board between the output and inverting
input pins. The frequency response is primarily determined by the feedback
resistor value, as described in Section 7.2.1. Increasing the value reduces the bandwidth, whereas decreasing
the value leads to a more peaked frequency response. The 1.24 kΩ feedback
resistor used in Section 5.8 is a good starting point for a gain of 10 V/V design.
- Connections to other wideband devices on the
board can be made with short direct traces or through onboard transmission
lines. For short connections, consider the trace and the input to the next
device as a lumped capacitive load. Relatively wide traces (50-mils to 100-mils,
0.050-in to 0.100-in, or 1.27-mm to 2.54-mm) must be used, preferably with
ground and power planes opened up around them.
- Socketing a high-speed part such as the THS6222 is not recommended. The additional lead
length and pin-to-pin capacitance introduced by the socket can create an
extremely troublesome parasitic network, and can make achieving a smooth, stable
frequency response almost impossible. Best results are obtained by soldering the
THS6222 directly onto the board.
- Use the VS– plane to conduct the heat
out of the package. The package attaches the die directly to an exposed thermal
pad on the bottom, and must be soldered to the board. This pad must be connected
electrically to the same voltage plane as the most negative supply voltage
(VS–) applied to the THS6222. Place
as many vias as possible on the thermal pad connection and connect the vias to a
heat spreading plane that is at the same potential as VS– on the
bottom side of the PCB.