SBOSA93C May 2023 – June 2024 OPT4001-Q1
PRODUCTION DATA
As listed in Table 6-4, the OPT4001-Q1 offers several conversion times that can be selected. Conversion time is defined as the time taken from initiation to completion of one measurement, including the time taken to update the results in the output register. Measurement initiation is determined by the mode of operation, as specified in Modes of Operation section.
CONVERSION_TIME REGISTER | TYPICAL CONVERSION TIME |
---|---|
0 | 0.6 ms |
1 | 1 ms |
2 | 1.8 ms |
3 | 3.4 ms |
4 | 6.5 ms |
5 | 12.7 ms |
6 | 25 ms |
7 | 50 ms |
8 | 100 ms |
9 | 200 ms |
10 | 400 ms |
11 | 800 ms |