SBOSAF5 April 2024 TMCS1126-Q1
PRODUCTION DATA
Nonlinearity is the deviation of the output voltage from a linear relationship to the input current. Nonlinearity voltage, as shown in Figure 7-1, is the maximum voltage deviation from the best-fit line based on measured parameters (see Equation 7).
where
Nonlinearity error for the TMCS1126-Q1 is specified as a percentage of the full-scale output range, VFS (see Equation 8).